Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Power Monitoring Expert 8.2 - How are database connection strings managed?
Issue
Power Monitoring Expert 8.2 - How are database connection strings managed?

Product Line
Power Monitoring Expert 8.2/9.0

Environment
Windows Registry

Cause
The way database connection strings are managed in the Windows Registry has changed significantly as of Power Monitoring Expert 8.2.

Resolution

Attached document highlights the changes in the Power Monitoring Expert database connection strings in the Windows Registry.

Schneider Electric Česká republika

Přílohy
PME82 Connection Strings.pdf [72.82 KB]