Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
For SSR relay, which EMC-relevant parts of the EN 61000 standard are met, in particular, is it part 1 + 3?
NO, there is no EMC declaration on our EU DOC certificate. See attached file, EU DOC - 2016  SSP3 SSM1 SSM2 SSL1 SSLZ.pdf.

Here is the reason, refer to IEC62314:2006 standard.

Solid state relays are components (not stand alone devices) and as such do not perform a
direct function. Therefore, no EMC requirements are included in this standard.

NOTE This is in line with the European EMC Directive.

Schneider Electric Česká republika

Přílohy
EU DOC - 2016 SSP3 SSM1 SSM2 SSL1 SSLZ.pdf [212.02 KB]