Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
RM17TU00 product, is there any technical differences between the old white version and the current black version product?
NO, there are no technical specification differences between the dark grey colour casing product and the old/previous cream colour casing product.

The reason we change the casing colour to dark grey is to standardize the products <Brand image> that we offer in the market.

All the recently launched products (example RE17, RE22 and RM22) are using this colour.