Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Have the Pedestal and Deadband been reversed on the Process Drives compared to the ATV61/71 drives?
Issue:
The Pedestal and Deadband appear to have been reversed on the Process Drives compared to the ATV61/71 drives.

Product Line:
ATV630, ATV930

Environment:
Pedestal and deadband

Cause:
n/a

Resolution:
Response from France:
We are aware about that and we are waiting for the solution.
Appears to be a problem on the keypad and SoMove.
Parameter BSP can have a setting of Standard, Pedestal, Deadband or Deadband 0 % :
When you see the Keypad: BSP can be standard , Deadband, pedestal or pedestal at 0%:
The term is inverted on keypad : Deadband should be Pedestal and pededstal /pedestal at 0% should Deadband/Deadband at 0%.
Same problem with SoMove:
The solution to set Pedestal like on ATV71, is to set Deadband on ATV6XX/ATV9xx.
We have asked for a solution on future softwares on the Keypad and SoMove.