Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How is a Jog function set up on the ATV630 Drives?
Issue:
Setting up jog function similar to the other Altivar Drives

Product line:
Altivar 630, Altivar 650, Altivar 660

Environment:
all

Cause:
n/a

Resolution:
A Jog function is not available on the Altivar 600 series drives. It is available on the 900 series drive.

If the VFD is set for 3-wire control, then change to the 900 series.
If the VFD is set for 2-wire control, then the Preset Speeds function may be acceptable.  Note that the Preset speed used for the jog speed will not run the motor at less than the Low Speed setting.