Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is there an OSHPD OPA or OPM for the anchorage detail in the document titled IBC Structural Calculations for Seismic Applications?
Issue:
OPA or OPM is being requested for the anchorage detail in the NetShelter structural calculations document.

Product line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
OPA or OPM is required.

Resolution:
The OSHPD Preapproval of Anchorage (OPA) was discontinued effective March, 1 2013.
OPM replaced OPA.
Installation of NetShelter SX cabinets using the bracket kit AR7701A-S, and following the instructions in the attached document, will be OSHPD approved.

NOTE: The IBC Structural Calculations for Seismic Applications document on the APC website will be updated soon to show the new bracket AR7701A-S is also to be used for IBC High Seismic Area installation.

Schneider Electric Česká republika

Přílohy
OPM-0255.pdf [1.21 MB]