Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the purpose of revenue metering and components of revenue metering in PM8000 series meters?

Issue
End user wants to understand revenue metering and how PM8000 series supports it.

Product line
PM8000 Series

Environment
Revenue Metering

Cause

Understanding revenue metering.

Resolution
The primary purpose of a revenue meter is to deliver measurements within industry-accepted accuracy limits over a defined operating range and to ensure protection against unauthorized alteration of these values. Compliance is governed by international standards (e.g., IEC, ANSI) and utility regulations.

PM8000 meters are certified for revenue metering and meet these requirements.

Components of Revenue Metering Security in PM8000:

  • Mechanical anti-tamper seals on the meter enclosure.
  • Password-based security for operations such as Peak Demand reset.
  • Hardware-based lock that prevents modification of revenue quantities once the meter is sealed.