Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How do you set up the analog input on the ATV630 and ATV930 for a current 0 to 20mA input?
Issue:
Analog input setup on the ATV630 and ATV930 for a current 0 to 20mA signal

Product Line:
ATV630 ATV930

Environment:
All

Cause:
Wants to set up AI1 for 0 to 20mA for speed control

Resolution:
Setting up AI1 as a 0 to 20mA input.

Using the HMI display

Go to the Main Menu
Go to the Complete settings
Go to the Inputs and outputs
Choose the 3rd function key black tab AI/AO
Go to the AI1 configuration
Go to AI1 type
Choose Current
Set AI1 min value to 0mA
Set AI1 Max value to 20mA.

Programming manual link

https://www.se.com/us/en/download/document/EAV64318/