Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How can I connect a XML Client to OFS V3.6?
After configuring COM / DCOM and IIS as specified in the User Manual, the user must add 2 more STEPS

Step 1: In “Internet Information Service (IIS)”  Add “Windows Authentication”
Access path:
Control Panel\All Control Panel Items\Programs and Features
Click in “Turn windows facture ON or OFF”
Select “Internet Information Service (IIS)” \World wide Web Services\Security
Select “Windows Authentication”

Step2:
Internet Information Services configuration on Windows x64 platforms
On x64 platforms, the IIS OFS application pool must have the property Enable 32-Bit applications set to TRUE.