Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
PowerSCADA Expert (PSE) 8.2 update #2 web client .cab file not found
Issue
After upgrading PSE PowerSCADA Expert 8.2 to update #2, the CitectSCADAWebClient_8_0_0_2078.cab cannot be found in default location c:\inetpub\wwwroot\citect\client\800

Product
PowerSCADA Expert 8.2 update #2

Environment
Windows explorer

Resolution
The .cab file is located in c:\inetpub\wwwroot\citect\client\750 on the PSE server. The web client is able to work with CitectSCADAWebClient_8_0_0_2078 selected without any additional work required.