Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Why, after assigning Dual Setting A/B (1 Wire) to Input 6, does Ecoreach change Input 5's assignment to None?
Issue:  IO1 Input 5 configuration getting set to "none" while configuring Dual settings Selection A/B (1 wire) through Ecoreach.

Product Line: IO Module, Ecoreach.

Cause:  Currently, every time a user assigns Dual Setting A/B (1 Wire) to Input #6, Ecoreach deliberately overrides the assignment for Input #5 to avoid possible conflicts between Inputs 5 and 6.

Resolution: ​Once Input #6 has been assigned to Dual Setting A/B (1 Wire), please configure the assignment for Input #5.