Jak vám dnes můžeme pomoci?

What is the meaning of “Diagnostic available through Modbus/TCP” for BMENOC03x1 using FC03?

Inside UP V12.0 Documentation looking for information relative to the "Diagnostic available through Modbus/TCP" for BMENOC03x1 we can see that a lot of diagnostic dedicated to these modules are available but not documented on this chapter.


But you can find all information relative to each of them going to (always inside Unity Pro Help)
>>the “Diagnostic available through Modbus/TCP” for 140NOC78x00 to get information on “Basic Network Diagnostics” and “Ethernet Port Diagnostics”
>> the “Modbus Diagnostic codes” for BMENOP0300 to get information on “SNTP Diagnostics”, “QoS Diagnostics” and “Identify”.