Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the UL50 type level for XB5PUSB, XB5PRJ45 equipped with cover?
The XB5PUSB* is certified UL 508 not UL50 (for types)
A cover should be used to get a type level according to UL50:
ZBSP1   --> Type 2
ZBSP2   --> no type
ZBSP3   --> Type 4
As these products are brand labelled, there is no direct proof of UL type
The only proof is the label with UL file and type (these labels are checked by UL Inspector in the factory)