Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Why does the ATV630 drive trip on EPF2 Fault after installing the BACnet Card?
Issue:
ATV630 getting an EPF2 Fault after installing the BACnet Card.

Product Line:
ATV600, ATV630, ATV660

Environment:
All

Cause:
NA

Resolution:
Check the Profile Setting. If it is set for I/O profile then change it to Separate or Not Separate. However, changing I/O profile puts you back to factory settings. Therefore, all the VFD settings have to be programmed again.