Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What would cause a SCF4 fault on the ATV320 drive?

Article available in these languages: Turečtina

Issue:
Causes of SCF4 fault on the ATV320 drive.

Product Line:
ATV320 drive

Environment:
All

Cause:
IGBT short circuit

Resolution:
SCF4 [IGBT short circuit] • Power component detected fault. • Contact Schneider Electric Product Support.
Troubleshooting check the motor and wiring to the motor.
Disconnect the motor turn off OPL and run the drive open circuit at 15 30 45 60hz
Running the Drive open circuit if the drive still fails then there is an issue with the drive.