Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Why does Vijeo Designer give me the warning "# instances of Vijeo Designer are already running"
Issue:
When launchng Vijeo Designer, a warning message appears stating that there are other instances already running.

Product Line:
Vijeo Designer (all versions)

Resolution:
When there are more than 3 instances of Vijeo Designer running, the software will warn you when you launch the 4th, 5th, ...etc instance thereafter. The purpose of this warning is to inform you that performance and resources will degrade as you launch more instances. This is just a warning and there is no negative effect to your application.

To avoid seeing this message, make sure to shut down Vijeo Designer when you are not using it.