ATV312 drive with a remote speed pot is working in reverse?
Reversed remote speed pot on an ATV312 drive.
Product Line:
ATV312
Environment:
All serial numbers
Cause:
Potentiometer is working backwards
Resolution:
Swap the +10vdc and the com terminal wires on the potentiometer to reverse the potentiometer operating direction.