Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Can Altivar drive ATV340 work in client-server communication via multidrive link?

Issue:
Can  Altivar drive ATV340 work in client-server communication via multidrive link?

Product Line:
ATV340 drives

Environment:
Multidrive link

Cause:
n/a

Resolution:
It's possible to make client/server via multidrive link on Altivat 340 since version V1.5IE10 and above.
The description and parameters are shown in Altivar 340 programming manual.
For full understanding and commissioning please contact local Schneider organization with the training request.