Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the BRA parameter in the Altivar Process Drive ATV630 and ATV930?
Issue:
BRA parameter in the Altivar Process Drive ATV630/930.

Product Line:
Altivar Process Drive ATV630, ATV930

Environment:
All serial numbers, all model numbers

Cause:
Customer wanted to adjust the deceleration ramp adaptation setting in the drives.

Resolution:
The BRA or dec.ramp adapt can be located by going to: Complete Setting -> Generic Functions -> Ramp -> DEC.Ramp Adapt.