Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is CSPN Certificate and which product are certified
CSPN (Certification de Sécurité de Premier Niveau) is a cyber security certification currently used
in the country of France. A product with CSPN certification can withstand a cyber attack driven by
2mmth of skilled hackers.

The M580 platform is CSPN-certified. BMEP58 CPU V2.20 or later & BMENOC0301/ BMENOC0311 V2.11 or later are certified.
Contact your local customer care center for more information.