Naše značky

Impact-Company-Logo-English Black-01-177x54

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Are the dimensions the same between ATV21 and ATV212 AC Drives of the same voltage and power rating?
Issue:
Is there a frame size difference between ATV21 and ATV212 AC Drives?

Product Line:
Altivar 212,
Altivar 21

Environment:
All models and serial numbers

Cause:
Mounting

Resolution:
There is no difference. The Altivar ATV21 and ATV212 frame sizes are exactly the same.