Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the IP rating for the Altivar Process Flange Kits?

Issue:
IP rating for VW3A95116.

Product line:
Altivar Process

Environment:
n/a

Cause:
Documentation does not show the IP rating.

Resolution:
The Flange kit is rated as IP40.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.