Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Unity Pro, how to create variables with a name having more than 32 characters.
Unity Pro allows name  of 32 charaters maximum for elementary variables
The solution to have more characters is to structure the variable using DDT.
By this way you will have nearly no more limitation  (it is possible to have nested DDT up to 15 levels).

Example:
Define the DDT variable

Intanciate the variable

use the variable: this variable has more than 32 characters