Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the concept of Ecostruxure Secure Connect Adviser?
What is the concept of Ecostruxure secure connect adviser
When you want to display or operate on a personal computer or smart device, the screens of display units in remote locations, you need a system to prevent unauthorized access from external sources. With EcoStruxure Secure Connect Advisor serving the role of router, as long as you have an Internet connection, you can construct such a system.


EcoStruxure Secure Connect Advisor is structured to connect safely display units on the work site (SiteManager), with computers or smart devices in the office (LinkManager), over a server (GateManager).

GateManager
Server for creating a safe encrypted connection between display units on the work site (SiteManager) and personal computers or smart devices in the office (LinkManager). You can use GateManager to check the network connection status of SiteManager and LinkManager. The GateManager Administrator registers the SiteManager and LinkManager and allows access to the network.

SiteManager
Display unit having SiteManager Embedded running is called SiteManager. Setup for accessing the network is handled from the software; SiteManager Embedded.

LinkManager
Software installed on the computers. It allows remote access to SiteManager and/or devices represented by agents on the SiteManager. Setup for accessing the network is handled by GateManager. For remote monitoring and operation, you can use data collection and remote monitoring software as the LinkManager.