Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Does M580 Safety PLC support the use of a BMXNOR0200H for Safety?
Issue
M580 Safety PLC support of a BMXNOR0200H

Product Line
M580 BMXNOR0200H

Environment
Unity Pro XLS, EcoStruxure Control Expert XLS

Resolution
For M580 safety PLC, the BMXNOR0200 or BMXNOR0200H modules are not classified as a safety certified modules and do not qualify as type-1 non-interfering modules.
However, the BMENOR2200H (note the extra 2)module is an type-1 non-interfering Ethernet type module that is safety certified.

The M580 Safety CPU allows the support of a maximum of four Ethernet type modules.