Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Com'X 510: Is it possible to simultaneously communicate on RJ-45 or screw terminals, Modbus RS-485 ports?

Issue

Simultaneous Modbus serial communication on RJ45 and removable screw terminal

Product line

Com'X 510 Energy Server

Environment

Meter Communication capability
Modbus Gateway
Modbus Master and Modbus Slave

Resolution

Com'X 510 Energy Server has 1 Modbus RS485 serial port consisting of an RJ45 and removable screw terminal connector (0 V, Screen, D0, D1).

Both connectors are plugged into the same Modbus RS485 serial port and can support 32 devices maximum.

The serial daisy chain or slave devices can be connected to either screw terminals or the RJ45 port, not both at the same time.

Com 'X 510

Refer to FA289876 for documentation for Com'X 510.