Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Can the stop button on the HMI be disabled as an E-stop when in terminal control mode on an ATV212?

Issue:
ATV212 stop button on the HMI disabling as an E-stop when in terminal control mode

Product Line:
ATV212, SFD212, SFD21

Environment:
All serial numbers

Cause:
Prevent "Flashing E" code. Prevent having to cycle power to clear the drive.

Resolution:
Stop/reset key.
The setting of parameter F734 determines whether it is possible to stop the drive by the Stop key which is located on the drive and graphic display option.
0 = [Enable]    1= [Disable]

Note:
LOSS OF CONTROL
You are going to disable the stop button located on the drive and graphic display option. Do not select 1 unless external stopping methods exist.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team. If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)