Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Which HV circuit breakers and contactors are Marine certified ?

The rated voltage for marine application and mainly on board the vessel are lower than 17.5 kV.
So the ranges which have been certified are :

- LF circuit breaker (SF6 technology)
- Evolis17 (vacuum technology)
- Rollarc contactor (SF6 technology)
- CVX /CBX contactor (vacuum technology)

The main certification body are :
- Bureau Veritas
- DNV.GL
- Lloyd's Register

The certificate should be renewed every two or three years.

The latest certificates may not uploaded in the Offer DAM which replace the Shopping KiosK.

If there's any request, please raise bFO cases for the latest one.