Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Can the HMIG3U play a sound file?
Issue:
Is it possible to play a sound file when an alarm occurs with the Magelis HMIG3U?

Product Line
HMIG3U

Environment:
Vijeo Designer V6.2 SP8

Resolution:
The HMIG3U can play sounds through the AUX port.  You will need to get this Schneider Electric connector HMIZGAUX.
The Speaker output on the AUX is rated for 300 mW (Rated Load: 8 Ω, Frequency: 1 kHz)
It supports sounds files that are 16-bit mono PCM or IMA ADPCM with 8, 12, or 16 kHz sampling rate. If you use a 11.025 kHz sound file on the HMIGTU, the file will play at 12 kHz.