Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
PowerChute Business Edition v10.0 Agent UI does not launch

Issue:
The PowerChute Agent web user interface (UI) does not launch using Google Chrome or Mozilla Firefox.

Product Line:
PowerChute Business Edition v10.0

NOTE: PowerChute Business Edition has been discontinued. We recommend discontinuing the use of PowerChute Business Edition and installing PowerChute Serial Shutdown. See https://www.se.com/us/en/product-range/137943580-powerchute-serial-shutdown#products

Environment:
Google Chrome v70+ and Mozilla Firefox v64+

Solution:

This issue was been resolved with the release of PowerChute v10.0.1.

Launch the PowerChute Agent UI in an alternative browser (e.g. Microsoft Edge). Upgrade the Java version used by PowerChute to OpenJDK v11.0.1, available to download on the OpenJDK website.

When the Java upgrade has successfully completed, launch the PowerChute Agent UI in Chrome or Firefox.

*** If you are experiencing an issue with PowerChute Business Edition 10.0.2, please review Schneider Electric FAQ 000208439 Cannot access the PowerChute Business Edition version 10.0.2 Agent web interface.