Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Where can I find detailed FAQ's on the import of the design file (.ELV file) in Ecoreach?
More help on the import of design file is integrated within Ecoreach. Follow the steps described below to find the help on importing the design file:
  1. From the Ecoreach home screen click on "Launch Device Discovery" option.
  2. On the "Add Devices" screen, select the option "Design project" from the drop down "Find Devices via:".
  3. Click the (?) icon on the top right corner of the screen to view the detailed FAQ on importing the design file in Ecoreach.