Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Does Schneider Electric offer a Class II, Division 2 HMI?
Issue:
Unable to find a Magelis HMI that is rated for Class II, Division 2 environments.

Product Line:
Magelis (XBTGT, XBTGK, XBTGH, HMISTO, HMISTU, HMIGTO, HMIGTU, HMIGK, iPC)

Resolution:
Schneider Electric HMI's under the Magelis product line are not rated for Class II, Division 2 environments. We currently do not have an offer for this application. We would suggest to put the existing HMI in an enclosure and control it using our Vijeo Design'Air app on a smart phone or tablet.