Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the part number for the conduit kits for the ATV630 and ATV930 drives?
Issue:
Conduit entrance kits for ATV630 drives.

Product Line:
Altivar Process

Environment:
Conduit Entrance kits

Cause:
n/a

Resolution:
For both ATV630 and ATV930 drives:
Frame Sizes 1-4 are supplied with the conduit kit already installed on the drives.
Frame size 5 drive are supplied with the conduit kit, but it does not come installed on the drive.
Frame size 6 drive is not supplied with the conduit kit.  Order separately, part number is VW3A9704.
Frame size 7 drive is not supplied with the conduit kit it, needs to be ordered separately.
***The part numbers are for frame size 7A (C22N4 drives) you need VW3A9212 and for frame size 7B (C25N4 and C31N4) you need VW3A9213.

See attachment for reference:



Schneider Electric Česká republika

Přílohy
ATV630 Conduit Entrance Kits.png [107.69 KB]