Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Does the ATV320 offer an Extended IO card?

Article available in these languages: japonština

Issue:
Extended IO Card for ATV320.

Product line:
Altivar 320 Machine drive

Environment:
all

Cause:
Customer needs additional Inputs and Outputs.

Resolution:
No, the ATV320 does not offer an extended IO Card.  Consider the ATV340, ATV630 or ATV930 drives which do have an extended IO option.