Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What can cause an EPF2 [Fieldbus Error] on an ATV340 and how to I correct it?
Issue:
Customer is experiencing an EPF2 [Fieldbus Error] on his ATV340 series drive.

Product line:
ATV340

Environment:
All

Cause:
An external error has been triggered via Fieldbus.

Resolution:
Remove the cause of the external error and then reset the fault by ether Auto Fault Reset, a manual fault reset assigned to a logic input, or by cycling power to the drive.