Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is it possible to call a DFB within another DFB with EcoStruxure Control Expert?

Issue:
Does EcoStruxure Control Expert allow to have nested DFB?  A DFB call within another DFB

Product Line:
EcoStruxure Control Expert

Resolution:
EcoStruxure Control Expert can have up to 15 level of nested DFB including DDT variables.   A DFB calling another DFB is considered a 2 layer nested DFB.