Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How to upload a program from an M251 controller
Issue:
How to upload a program from an M251 controller

Product Line:
M251

Resolution:

Note:
  • Upload from any M2xx PLC is only possible if the project archive had been downloaded to the PLC by the person that programmed the PLC.   Download of the archive is an elective choice and not automatic. The project is the programmers intellectual property so it's up to the programmer to decide if they want to save a copy of the archive to the PLC. Assuming the project archive has already been downloaded to the PLC, the following procedure may be followed.

- Start by launching SoMachine
- Select 'Connect Controller'
- If controller is powered and connected by USB, it shows up in the list.
- Select it and click 'Upload project from controller'
- Select where to save the uploaded file on your PC and select 'Yes' to open it.
- You can now access the project code