Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How to Change the Password for FlexNet Publisher
Issue
The user would like to change the password for FlexNet Publisher due to security reasons.

Product Line
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020

Environment
License Manager
Floating License Manager
FlexNet Publisher

Cause
The customer would like to know how to change the password for FlexNet Publisher.

Resolution
  1. To navigate to the FlexNet Publisher page, type "http://localhost:8090" on the PME server.
  2. On the top right, click on the "Administration" tab.
  3. The default username and password are "admin" and "admin", respectively. *If the current password is unknown, refer to FA230648 to reset to the default password*.
  4. On the "System Information" tab, there is an option at the bottom to "Change Password"
  5. No services are required to restart for the change to take effect.