Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What web services are supported by BMXNOR0200 when used as SOAP (Simple Object Access Protocol) server
Issue:
What web services are supported by BMXNOR0200 when used as SOAP (Simple Object Access Protocol) server

Product Line:
BMXNOR0200H

Environment:
All

Resolution:

Two kinds of Web services are provided in BMXNOR0200H modules as SOAP server interfaces:

1) ModbusXMLDA: Web service to implement data access to Modbus variables,
2) SymbolicXMLDA: Web service to implement Symbolic data access.

The Web services provided by BMXNOR0200Hare compatible with the WS-I basic profile 1.1.