Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Hierarchy Manager - cannot see the entire list of physical meters comprising a virtual meter when you try to edit the virtual meter
Product LIne
Power Monitoring Expert 8.x
Power Monitoring Expert 9

Environment
Hierarchy Manager

Issue
In Hierarchy Manager, create a virtual meter that includes more than four physical meters in google chrome and you select edit to see that virtual meter, the last one is always unreadable.
The scroll bar does not seem to be working properly.
It works perfectly in Internet Explorer and we experience this issue only in google chrome.

Resolution
  • Use Internet Explorer or
  • You can click on Add (as if you are adding a new meter) and the window that pops up shows the entire list of the physical meter with a proper scroll bar.