Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Where is the 24Vdc internal power supply terminal for digital inputs on the ATV340U07N4E drive?
Issue:
Does the ATV340 has internal 24Vdc control voltage for digital inputs?

Product Line:
ATV340

Environment:
ATV340 frame sizes 1 - 3

Cause:
Customer didn't see 24Vdc input on the terminal block.

Resolution:
The 24Vdc input is labeled as DISUP.
s
The 24VDC supply can be checked by measuring between DISUP and either of the COM terminals.