Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How to read the variables defined in Program Unit via OFS?
  1. Issue
How to read the variables defined in Program Unit via OFS?
  1. Product Line
Control Expert V14.0, OFS V3.62
  1. Environment
Control Expert V14.0, OFS V3.62, M580
  1. Resolution
Only the variables defined in the global project can be read via OFS.
But if you define the variables in Program Unit as external variables with the same and data type as the ones defined in the global project, then you can read the variable in OFS Client.




Additionally, it is disabled to select the attribute HMI variable for the variables defined in Program Unit.
OFS.png