Jak vám dnes můžeme pomoci?

Cannot create projects in Control Expert after activating the Security.

Issue
Cannot create projects in Control Expert after activating the security from within the 'Security Editor'.

Product Line
Control Expert

Environment
Windows 10, Windows 7

Resolution
Attempts to create a new Control Expert application fails after enabling security.

This issue will occur if the 'DTM Access' is defined as 'SystemOperator in security profile..
hyt


To resolve the issue, change the 'DTM Access rights' to 'Administrator'.
tyhyt