Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Easergy P5 Virtual Injection: How can I enable the virtual injector in eSetup Easergy PRO?
The virtual injection functionality is available only on-line, when the device is connected to a PC using a USB cable. Then the virtual injection window will appear on the right-hand side of Easergy Pro screen.

After connecting to your relay and logging in with Easergy PRO, the user needs to change the mode of the device to ‘Test’ or 'TestBlocked.'