Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
When trying to write the settings file to a MiCOM Px30 relay is outputs the following message “The following settings can be sent individually only.”
Issue
When trying to write the settings file to a MiCOM Px30 relay is outputs the following message “The following settings can be sent individually only.”

Product Line
MiCOM P30 Range

Environment
Easergy Studio

Cause
Need to know if the full settings file can be sent to the MiCOM relay.

Resolution
Whenever a settings file is sent to a MiCOM Px30 device, a prompt always appears warning the user that several settings cannot be sent in the file, and that they have to be sent individually. It is the user's responsibility to go through the list of settings that can only be sent individually and send to the MiCOM relay those that are needed. The settings that are not being used can be ignored. This is normal behavior for all MiCOM Px30 relays. There is no way to send the entire settings in one command.