Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
PME - Adding Offset to the Register Power Monitoring Expert Device Type Editor
Issue:
In PME Device Type Editor, there is no section displayed by default to add Offset for Modbus Registers.

Product Line:
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment:
Device Type Editor

Resolution:
1. Open Management Console > Tools > System > Device Type Editor
2. File > Open the translator you want to edit
3. Right-click one of the default columns (i.e. Name, Register, Format, ION Handle, Mask, Scale) and select Column Chooser

Right-click column headersand select Column Chooser

4. Scroll to find "Offset" and drag the Offset onto the column headers

Select Offset