Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
PM5000 - From where to get EAC Certificate without the watermark?
The EAC certificates without watermark can be shared only with the Custom Team due to the <<Stop gray procedure>>.
So the customer needs to request the Custom department to put a request directly to the EAC team to get the certificate without the watermark. Any such request directly from the end-user is not accepted.