Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
ION8650 Power supply connection-Auxiliary power Pigtail
Issue

Please confirm the plug definition for DC power supply of ION8650? I cannot confirm it base on installation guide.
Which pin is L/+, which is N/- ?
8650_1

2

In our installation guide, only have this info but no details.

3




Answer:
Please check the following picture for the details of Which pin is L/+ and N/-:
4