Jak vám dnes můžeme pomoci?

How to set the dial in Tesys U Motor starters?

Issue:
Do Tesys U Motor starters take into account the service factor?

Product Line:
Contactors and Starters-IEC

Environment:
Tesys U Motor starters

Resolution:
— If the motor has a 1.0 service factor, multiply the motor full-load current by 0.9 and adjust the dial to that number.
— If the motor has a 1.15 to 1.25 service factor, set the adjustment dial to the motor full-load current.