Jak vám dnes můžeme pomoci?

What is CF12 fault on the ATV600 and ATV900 Process drives?

Issue:
What can cause a CF12 fault on the ATV600 and ATV900 Process drives?

Product Line:
ATV600 and ATV900

Environment:
All

Cause:
Corrupt file in HMI

Resolution:
"Conf transfer Error"
Principle:
The Configuration transfer error occurs if a configuration file could not be loaded to the device, or the config. is not compatible with the drive.
Probable cause:
• The configuration transfer to the drive was not successful or interrupted.
• The stored configuration (HMI) was loaded from an different firmware (MCP/MCE)
Remedy:
• Load a compatible configuration.
• Use SoMove to transfer configuration to an other drive.
• Perform a factory setting"